ProxyStructMonitorAlarmClassDesc (STRUCT)
TYPE ProxyStructMonitorAlarmClassDesc : STRUCT
This structure is used to store the description of an alarm class
- InOut:
Name
Type
Comment
sNameSTRINGThe name of the alarmclass
udiInternalIDUDINTThe internal id of the alarmclass
usiPriorityUSINTThe priority of the alarmclass
xAcknowledgeSeparatelyBOOLThe flag, that indicates, whether alarms referencing this alarm class have to be acknowledged separately [return value of IAlarmClass.IsAcknowledgeSeparately()]