SolarModeManual (FB)
FUNCTION_BLOCK SolarModeManual EXTENDS AbbLConC3
This function block represents an operation mode that allows the system to set in manual mode. User can move the system by using drives directly. While this mode is active, the system will not respond to any commands from the solar control field.
- InOut:
Scope
Name
Type
Initial
Comment
Inherited from
Input
EnableBOOLFALSE
A rising edge (Enable = TRUE) starts the operation, the output Busy goes to TRUE. All other inputs are read and considered continuously. Execution will continue forever until a falling edge (Enable = FALSE) aborts the operation. During Aborting the Busy is still TRUE. Afterward all outputs are reset.
AbbLConC3
Output
BusyBOOLFALSE
Operation is running (while output Error is FALSE)
AbbLConC3
ErrorBOOLFALSE
Operation is stopped with error (while output Busy is FALSE). This output is TRUE for at least one cycle or until Enable is set to FALSE. The output ErrorID gives more details about the error.
AbbLConC3
Input
ManualFwdBOOLFALSE
2: In order to move manually the system forward, input is set to TRUE
ManualBwdBOOLFALSE
3: In order to move manually the system backward, input is set to TRUE
Inout
GoToPosRefBOOL4: Boolean expression that enables position control block
PosRefREAL5: Desired position to locate the tracker.
JogFwdBOOL6: Indicates drive is running forward
JogBwdBOOL7: Indicates drive is running backward
Output
ErrorIDNO_ERROR
3: Error code
Methods:
A_StartAction
B_CyclicAction
C_CleaningAction
D_AbortAction
E_ResetAction
Structure: