ComGetCaaSerialComConfig (FB)

FUNCTION_BLOCK ComGetCaaSerialComConfig EXTENDS AbbETrig

Obtain configuration data of project for a specified COM port in CAA SerialCom compatible format^

InOut:

Scope

Name

Type

Initial

Comment

Inherited from

Input

Execute

BOOL

FALSE

A rising edge starts the operation, the output Busy goes to TRUE. In the first cycle all other inputs are read and stored, afterwards they are ignored. A falling edge does not stop the operation. After Done = TRUE or Error = TRUE and Execute = FALSE all outputs will be reset.

AbbETrig

Output

Done

BOOL

FALSE

Operation is completed without error (while outputs Busy and Error are FALSE). This output is TRUE for at least one cycle or until Execute is set to FALSE

AbbETrig

Busy

BOOL

FALSE

Operation is running (while outputs Done and Error are FALSE)

AbbETrig

Error

BOOL

FALSE

Operation is stopped with error (while outputs Busy and Done are FALSE). This output is TRUE for at least one cycle or until Execute is set to FALSE. The output ErrorID gives more details about the error.

AbbETrig

Input

ComID

COM_PORT_ID

COM_PORT.COM_ID_INVALID

COM port ID: Use ComGetIdByName() to get the COM port ID for a serial device as shown in the configuration device tree

pCaaParamList

POINTER TO Serial_Communication.COM.PARAMETER

0

Where configuration data will be written to

NumParams

UINT

0

Number of available elements in pasCaaParamList

Output

ErrorID

ERROR_ID

ERROR_ID.NO_ERROR

Error code describing error condition