PmpEnergyCalc (FB)

FUNCTION_BLOCK PmpEnergyCalc EXTENDS AbbLConC3

Only to be used when station has VFD based pumps. This function block calculates the energy consumed and saved. Based on that, the CO2 emission reductions and money saved is also computed. The Function block PmpEnergyCalc calculates the energy consumption of the pumping station run by variable frequency drive and gives the information on cumulative flow in cubic meters. The Function Block includes following calculations:

  • Total energy consumed

  • Total energy saved

  • Total cost saved

  • Reduced CO2 emission

Note

For correct calculations this function block must be called in the task manager with 50 ms cyclic time.

InOut:

Scope

Name

Type

Initial

Comment

Input

Start

BOOL

FALSE

2: To start the Energy calculation.
  • When input is TRUE, the execution starts.

  • When input is FALSE, the execution stops if running.

Tariff

REAL

1.0

3: Per kWhr tariff rate in terms of currency, e.g. Dollar, Euro etc. Range-Value>0.0

CO2Conversion

REAL

1.0

4: Factor which helps in converting the energy consumed in terms of CO2 emission tn/MWh. Range-Value>0.0

MonitorDuration

INT

10

5: Time duration in minutes, to monitor the energy consumption. Range-Value>0

PumpFlow

ARRAY [1..4] OF REAL

6: Actual flow of each pump in m3/hr. Range-Value>0.0

Note

The index 1 array is connected to the PumpID = 1. This pattern follows for all pump IDs.

PumpRatedPower

ARRAY [1..4] OF REAL

7: Rated power in kW of each pump, if directly connected to the motor. Range-Value>0.0

PumpActPower

ARRAY [1..4] OF REAL

8: Actual power of each pump in kW. Read from the VFD.Always PumpActPower < PumpDOLPower. Range-Value>0.0

ResetTotalVolume

BOOL

FALSE

9: Reset Total volume.
  • When input is TRUE, total volume is reset.

  • When input is FALSE, pump continues with total volume.

ResetTotalEnergy

BOOL

FALSE

10: Reset Total Energy.
  • When input is TRUE, total energy value is reset.

  • When input is FALSE, pump continues with total energy value.

PmpStationParameters

PmpStationType

11: Pump Station structure which stores pumping station data.

Inout

TotalVolume

LREAL

12: Cumulative Flow Volume in Cubic meters. Total volume which is calculated using flow of all the pumps, in m3.

TotalEnergy

LREAL

13: The variable input/output TotalEnergy indicates the total actual energy in kWh.
  • The total energy is calculated by combining the actual power of all pumps in kW in a hour.

Output

ErrorID

ERROR_ID

3: Error code in case of error in the function block execution.

EnergyConsumed

REAL

0.0

4: Indicates energy consumed in the monitoring duration, in kWh. Value>=0.0

EnergySaved

REAL

0.0

5: Indicates energy saved, in kW. Difference of energy consumed by pump with VFD and pump with DOL. Value>=0.0

MoneySaved

REAL

0.0

6: Money saved, in tariff units. Value>=0.0

CO2Reduction

REAL

0.0

7: Reduction of carbon dioxide emissions, in tn/MWh. Value>=0.0

Methods:

A_StartAction

B_CyclicAction

C_CleaningAction

D_AbortAction

E_ResetAction

Structure: