ERROR_ID (ENUM)
- TYPE ERROR_ID(
NO_ERROR
Enumeration of the Error ID, describes the details of each Error ID generated by library function blocks.
- InOut:
Name
Initial
Comment
NO_ERROR
0
zLOG_ERROR_NO_TYPE_SPECIFIED
29184
errorcodes 7200hex … 727Fhex
zLOG_ERROR_SQ_OUTSIDE_VALID_RANGE_0_TO_31
zLOG_ERROR_LENGTH_BOOL_EXCEEDED_MAX_LENGTH_58
zLOG_ERROR_LENGTH_BYTE_EXCEEDED_MAX_LENGTH_88
zLOG_ERROR_LENGTH_INT_EXCEEDED_MAX_LENGTH_50
zLOG_ERROR_LENGTH_UINT_EXCEEDED_MAX_LENGTH_58
zLOG_ERROR_LENGTH_DINT_EXCEEDED_MAX_LENGTH_29
zLOG_ERROR_LENGTH_UDINT_EXCEEDED_MAX_LENGTH_31
zLOG_ERROR_LENGTH_REAL_EXCEEDED_MAX_LENGTH_27
zLOG_ERROR_OPEN_ERR
zLOG_ERROR_GETPOS_ERR
zLOG_ERROR_SETPOS_ERR
zLOG_ERROR_WRITE_ERR
zLOG_ERROR_READ_ERR
zLOG_ERROR_CLOSE_ERR
zLOG_ERROR_GETSIZE_ERR
zLOG_ERROR_FLUSH_ERR
zLOG_ERROR_MAX_NUMBER_OF_FILES_EXCEEDED
zLOG_ERROR_MAX_NUMBER_OF_DATASETS_PRO_FILE_EXCEEDED
zLOG_ERROR_FILE_WRITE_FAILED
zLOG_ERROR_FILE_READ_FAILED
zLOG_ERROR_FILE_MOVE_COPY
zLOG_ERROR_CREATE_DIRECTORY
zLOG_ERROR_FILE_MOVE_DELETE
zLOG_ERROR_NO_CSV_FOUND_IN_DATASET
zLOG_ERROR_DELETE_ACTUAL_FILE
zLOG_ERROR_FORMAT_DISK1
zLOG_ERROR_FORMAT_DISK2
zLOG_ERROR_DELETE_ACTUAL_FILES_NO_FILE_FOUND
zLOG_ERROR_DELETE_SAVE_FILES_NO_FILE_FOUND
zLOG_ERROR_ILLEGAL_MODE
zLOG_ERROR_ILLEGAL_DESIGNATION_ON_DISK1
zLOG_ERROR_ILLEGAL_DESIGNATION_ON_DISK2
zLOG_ERROR_FORMAT_NOT_SUPPORTED
zLOG_ERROR_MODE3_AND_DISK2_EXTENSION_TRUE_NOT_ALLOWED
zLOG_ERROR_PARAMETER_THRESHOLD_CPY_FIFOIN_TO_FILE_MAX_120
zLOG_ERROR_IEC60870_SEND_M_SP1_ET
zLOG_ERROR_IEC60870_SEND_M_SP16_ET
zLOG_ERROR_IEC60870_SEND_M_DP_ET
zLOG_ERROR_IEC60870_SEND_M_IT1_ET
zLOG_ERROR_IEC60870_SEND_M_IT16_ET
zLOG_ERROR_IEC60870_SEND_M_ME1_ET
zLOG_ERROR_IEC60870_SEND_M_ME16_ET
zLOG_OVERFLOW_IEC60870_SEND_M_SP1_ET
zLOG_OVERFLOW_IEC60870_SEND_M_SP16_ET
zLOG_OVERFLOW_IEC60870_SEND_M_DP_ET
zLOG_OVERFLOW_IEC60870_SEND_M_IT1_ET
zLOG_OVERFLOW_IEC60870_SEND_M_IT16_ET
zLOG_OVERFLOW_IEC60870_SEND_M_ME1_ET
zLOG_OVERFLOW_IEC60870_SEND_M_ME16_ET
zLOG_ERROR_TIMEOUT_DIRECTORY_CREATE_FILE_MOVE
zLOG_ERROR_RESERVE
zLOG_ERROR_TIMEOUT_FILE_DELETE
zLOG_ERROR_TIMEOUT_DISK_FORMAT
zLOG_ERROR_TIMEOUT_WRITE_DATASET_IN_FILE
zLOG_ERROR_TIMEOUT_READ_DATASET_IN_CASE_OF_CONNECT
zLOG_ERROR_TIMEOUT_WRITE_DATASET_IN_CASE_OF_CONNECT
zLOG_ERROR_TIMEOUT_READ_DATASET_IN_CASE_OF_NOT_CONNECT
zLOG_ERROR_TIMEOUT_IEC60870_COMMUNICATION
LOG_ERROR_LIBRARY_IS_NOT_SUPPORTED_IN_THIS_PLC_TYPE