EtherCatReconfigure (FB)

FUNCTION_BLOCK EtherCatReconfigure EXTENDS AbbETrig

Reconfigure EtherCAT master device

InOut:

Scope

Name

Type

Initial

Comment

Inherited from

Input

Execute

BOOL

FALSE

A rising edge starts the operation, the output Busy goes to TRUE. In the first cycle all other inputs are read and stored, afterwards they are ignored. A falling edge does not stop the operation. After Done = TRUE or Error = TRUE and Execute = FALSE all outputs will be reset.

AbbETrig

Output

Done

BOOL

FALSE

Operation is completed without error (while outputs Busy and Error are FALSE). This output is TRUE for at least one cycle or until Execute is set to FALSE

AbbETrig

Busy

BOOL

FALSE

Operation is running (while outputs Done and Error are FALSE)

AbbETrig

Error

BOOL

FALSE

Operation is stopped with error (while outputs Busy and Done are FALSE). This output is TRUE for at least one cycle or until Execute is set to FALSE. The output ErrorID gives more details about the error.

AbbETrig

Input

Device

IDeviceCM579EtherCAT

EtherCAT master device

TargetState

AC500_EtherCAT.AC500_EcatBase.teEcatDevState

Target state of ECAT master to be entered after it has been configured successfully

SkipENICreation

BOOL

Do NOT create a new ENI-file but instead use an existing one

ScannedDevicesCount

UINT

Number of devices found by scan

Output

ErrorId

ErrFlexConf

Indicates details of error of reconfiguration

Input

BusDeviceOrder

POINTER TO WORD

List of physical adresses of slave devices in the same order as found on the bus. Attention: Content gets modified by FB execution!

ScannedDevices

POINTER TO AC500_EtherCAT.AC500_NetxEcat.tsNetxEcatBusScanDeviceInfo

List of devices as found on the bus