ERROR_ID (ENUM)
- TYPE ERROR_ID(
NO_ERROR
- Attributes:
qualified_only- InOut:
Name
Initial
Comment
NO_ERROR
0
No error
EMPTY_STRING
1
Device name string is empty
SLOT_NUM_ERR
2
Slot number not allowed
DATA_SIZE_INVALID
3
Data size is not the expected one
IM0_LENGTH_ERR
4
IM0 length error
INVALID_POINTER
5
Invalid pointer found
SLOT_OR_DEV_HANDLE_ERR
6
Slot Error or no Device handle
NO_CONF_CMD_RECEIVED
7
No confirmation on request
NO_NETX_CHNL_FOR_SLOTADDR
8
No valid Netx channel on coupler slot
JOB_NOTCREATED
9
No job created
UDISTA_ERR
10
More stack errors possible, further information, if avaiable in output AddErrNo
ASYNC_STATE_BAD
11
Job finished but bad
JOB_RESULT_ERR
12
Job result error, further information in output AddErrNo
STARTJOB_FAULTY
13
Job could not be started
UNKNOWN_ERROR
100
An unknown error occurred
FATAL_ERROR
16#5FFF
Fatal error of model state machine