ERROR_ID (ENUM)
- TYPE ERROR_ID(
NO_ERROR
- Attributes:
qualified_only- InOut:
Name
Initial
Comment
NO_ERROR
0
no error
FAILED
1
general error
INVALID_DEVICE_INSTANCE
2
no or invalid device assiged at input Device
DATA_LENGTH_TOO_BIG
3
Length of command data too big, maximum value is 8
RESPONSE_DATA_LENGTH_TOO_BIG
4
Length of response data too big, maximum value is 8
RESPONSE_DATA_LENGTH_TOO_SMALL
5
Length of response data too small, minimum value is 1
INVALID_RESPONSE_DATA
6
Invalid data of command response
INVALID_RESPONSE_LENGTH
7
length of response data doesn’t match with expected length
NO_RESPONSE_RECEIVED
8
no response from device received
COMMAND_TIMEOUT
9
command wasn’t processed within expected time
FATAL_ERROR
16#5FFF
fatal error of model state machine