PmRealtimeClockDT (FB)
FUNCTION_BLOCK PmRealtimeClockDT EXTENDS AbbLConC3
This function block allows to set and display the current time and date in DT format.
- InOut:
Scope
Name
Type
Initial
Comment
Inherited from
Input
EnableBOOLFALSE
A rising edge (Enable = TRUE) starts the operation, the output Busy goes to TRUE. All other inputs are read and considered continuously. Execution will continue forever until a falling edge (Enable = FALSE) aborts the operation. During Aborting the Busy is still TRUE. Afterward all outputs are reset.
AbbLConC3
Output
BusyBOOLFALSE
Operation is running (while output Error is FALSE)
AbbLConC3
ErrorBOOLFALSE
Operation is stopped with error (while output Busy is FALSE). This output is TRUE for at least one cycle or until Enable is set to FALSE. The output ErrorID gives more details about the error.
AbbLConC3
Input
SetBOOLFALSE
FALSE/TRUE edge sets the time and date
DTSetDTDATE_AND_TIME#1970-1-1-0:0
Set input for date and time in DT format
Output
ErrorIDERROR_ID.NO_ERROR
Error code describing error condition
DTActDTDATE_AND_TIME#1970-1-1-0:0
Actual date and time in DT format