teErrorCodesOB (ENUM)
- TYPE teErrorCodesOB(
eOK
- Attributes:
qualified_only- InOut:
Name
Initial
Comment
eOK
0
eWrongBoard
1
Wrong board or none is plugged in slot
eBoardDefective
2
Correct board but faild to gain access
eBoardDirection
3
Correct board found but failed to set directions (Internal Error)
eBoardParameter
4
Parameter was faulty (Only Run On Config Fault)
eFailureOnParameterValue
5
Parameter value Product failed
eFailureAddress
6
I2C failed to set address
eFailureRead
7
I2C failed to read
eFailureWrite
8
I2C failed to write
eNone
255
Dummy to end list