IoDrvDNP3 (LIB)
Description 1
This is the IO Driver based DNP3 Outstation library which enables the DNP3 Outstation features in the AC500 PLCs. This library contains function blocks and functions which are configured from Automation builder, this is an internal library and automatically when DNP3 is configured under a PLC.
Copyright: We reserve all rights in these programs and the information therein. Reproduction, use or disclosure to third parties without express authority is strictly forbidden. (c) 2006-2024 ABB, all rights reserved
Contents:
Indices and tables
- 1
- Based on ABB_IoDrvDNP3_AC500.library, last modified 29.10.2025, 13:07:30. LibDoc 4.6.0.0-r.29The content file ABB_IoDrvDNP3_AC500.json was generated with Automation Builder 2.9 on 29.10.2025, 13:07:53.