Gateway configurationPermalink

  1. In the Automation Builder project, right-click the topmost PLC tree node and select “Communication Settings”.

    The dialog window “Communication Settings” appears.

  2. Click “Advanced Settings” to open the dialog.

    ⮫ “Tab 'Communication Settings'”

    This information is stored in the project file.

  3. Click “Gateway” and select the desired action from the “Gateway” menu to change the local gateway or to add a new gateway channel.

    ⮫ “Command 'Configure the Local Gateway'”

    ⮫ “Command 'Add New Gateway'”

    Click [OK] to confirm the settings.