Command 'Add New Gateway'Permalink

Function: This command opens the “Gateway” dialog where you can define a gateway channel and add it to the current device configuration.

Call: Menu bar: “Gateway” in the “Communication Settings” dialog of the device editor.

Dialog 'Gateway'

“Name”

Name of the gateway.

“Driver”

Driver type from a drop-down list.

Driver-specific settings, for example:

IP address, port

Editable after double-clicking the predefined value. A short description for each parameter is displayed in the lower part of the dialog.

Note: You can also specify the address of a DNS domain. This has to begin with ‎dns:‎ (example: ‎dns:MyDynDNSAdress‎).

The dialog is also used for later editing of the gateway entries of your project.