DrvControlACSPermalink

DrvControlACS
Overview_of_DrvControlACS

This function block can be used to control ACS drives with ABB drives profile using direct input of status word (SW) from drive via any supported fieldbus communication like PROFINET, EtherCAT, CANopen.

Control word (CW) will be built by the function block according to the ABB drives profile state machine. Output CW has to be send to the drive via any fieldbus communication supported. Function block provides standard start/stop signals to control the drive and standard diagnosis signals are read from the drive.

Drive Parameter

ACS380/ ACS480/

ACS580/ ACH580/

ACQ580/ ACS880

ACSM1

Comment

EXT1 COMMANDS

20.01 = Fieldbus A

10.01 = FBA

Fieldbus interface as source for start and stop

EXT1 / EXT2 SEL

19.11 = MCW Bit11 (06.01)

34.01 = P02.12 bit 15

Fieldbus interface as source to switch to EXT2 control place

REF1 SELECT

22.11 = FBA ref1

24.01 = FBA ref1

Fieldbus interface as source to speed reference

FAULT RESET SELECT

31.11 = P06.01 bit 7

10.08 = P02.12 bit 8

Fieldbus interface as source for fault reset

PROFILE

51.02 = Drives Classic / Enhanced

51.02 = Drives Classic / Enhanced

Control profile to ABB Drives profile classic or enhanced