The PROFINET IO devices combine the advantages of decentralized I/O modules with the reaction time of AC500 mounted central I/O modules. The devices for PROFINET provide the extension -PNIO in the device name.
The communication module CM579-PNIO acts as I/O controller in a PROFINET network. It is connected to the processor module via an internal communication bus. Depending on the terminal base, several communication modules can be used for one processor module.
The communication interface modules CI5xx-PNIO act as I/O devices in a PROFINET network.
Additionally the communication module CM589-PNIO(-4) can be used to setup a AC500 PLC to act as I/O module in a PROFINET network.
The difference of the CI5xx-PNIO devices can be found in their input and output characteristics⮫ “Characteristics of CI50x-PNIO”.
-
Characteristics of CI50x-PNIO
-
Input/Output characteristics of CI501-PNIO
-
Input/Output characteristics of CI502-PNIO
-
Technical data of the serial interfaces of CI504-PNIO