Version informationPermalink

Information about the installed Automation Builder version, such as installed packages or license terms, is available via “Help  About”.

About_Box_ready

Package version information

Displays all installed software packages.

Plug-in version information

Displays all installed plug-ins.

Safety version information

Displays all installed safety components (visible only if the safety option is installed).

User registration data

Allows entering or updating registration information.

License Terms

Shows license terms.

Create package for support

Creates a package that can be saved or sent to support.

⮫ “Create log files for support”

It is possible to continue working with a project in an older Automation Builder version or to update a project to the latest Automation Builder version.