'Online' 'Sourcecode download'Permalink

This command loads the source code for the project into the controller system. This is not to be confused with the Code that is created when the project is compiled! You can enter the options that apply to Download (time, size) in the 'Project' 'Options' 'Source download' dialog.

⮫ “'Project' 'Options'”

⮫ “'Source download'”