'Project' 'Options'Permalink

With this command the dialog box for setting options is opened. The options are divided into different categories. Choose the desired category on the left side of the dialog box by means of a mouse click or using the arrow keys and change the options on the right side.

An image of the options which are set for the current project, will be found in the Resources tab in component Workspace.

⮫ “Workspace”

The settings amongst other things serve to configure the view of the main window. They are, unless determined otherwise, saved in the file "codesys.ini" and restored at the next startup.

You have at your disposal the following categories:

Category 

Stored in AC500-S Programming Tool

Stored in project

Load & Save

⮫ “Options for load & save”

x

 

User information

⮫ “Options for user information”

x

 

Editor

⮫ “Options for editor”

x

 

Desktop

⮫ “Options for the desktop”

x

 

Color

⮫ “Options for colors”

x

 

Directories

⮫ “Options for directories”

Cat. Common

Cat. Project

Log ⮫ “Options for log”

x

 

Build

⮫ “Options for build”

 

 

Passwords

⮫ “Passwords”

 

 

Source download

⮫ “'Source download'”

x

 

Symbol configuration

⮫ “Options for 'Symbol configuration'”

x

 

Project Source Control

⮫ “Options for 'Project source control'”

 

x

Macros

⮫ “Options for 'Macros'”

 

x