OptionsPermalink

The “Options” command of the “IEC61850” category opens a dialog for the setting of different display options for the IEC 61850 configurator.

Option

Description

“Show FC besides data attribute”

Display option, shows functional constraint of attribute as a comment.

“Show type besides data attribute”

Display option, shows type of attribute as a comment.

“Show trigger option besides data attribute”

Display option, shows trigger option of attribute as a comment.

“Show description besides data objects”

Display option, shows description of attribute as a comment.

“Enable SCL Private block”

“Select all Data Objects”

Debug-Option: Selection of all data objects (DO).

“Select all Data Attributes”

Debug-Option: Selection of all data attributes (DA).