Generate codePermalink

Symbol: SY_2022_CS_generated_icon

On activating the “Generate code” command of the “IEC61850” category the code generation is started and the generated IEC 61850 code is stored in the folder “IEC61850 Generated POUs” in the device tree.

⮫ “Generate IEC61850 code”