Shortcut: <Ctrl>+<P>
With this command the content of the active window is printed.
After the command has been chosen, then the Print dialog box appears. Choose the desired option or configure the printer and then click OK. The active window is printed. Color output is available from all editors.

You can determine the number of the copies and print the version to a file.
With the button 'Properties' you open the dialog box to set up the printer.
You can determine the layout of your printout with the command 'File' 'Printer setup'.
During printing the dialog box shows you the number of pages already printed. When you close this dialog box, then the printing stops after the next page.
In order to document your entire project, use the command 'Project' 'Document'.
If you want to create a document frame for your project, in which you can store comments regarding all the variables used in the project, then open a global variables list and use the command 'Extras' 'Make docuframe file'.