This command lets you print the documentation of your entire project.
The elements of a complete documentation are as follows.
-
The POUs
-
The contents of the documentation
-
The datatypes
-
The visualizations
-
The resources, global variables, variables configuration, the Sampling Trace, the PLC Configuration, the Task Configuration, the Watch and Receipt Manager)
-
The call trees of POUs and data types
-
The cross-reference list
For the last two items the project must have been built without errors.

Only those areas highlighted in blue in the dialog box are printed.
If you want to select the entire project, then select the name of your project in the first line.
If, on the other hand, you only want to select a single object, then click on the corresponding object or move the dotted rectangle onto the desired object with the arrow key. Objects which have a plus sign in front of their symbols are organization objects which contain other objects. With a click on a plus sign organization object is expanded, and with a click on the resulting minus sign it can be closed up again. When you select an organization object, then all relevant objects are also selected. By pressing the <Shift> key you can select a group of objects, and by pressing the <Ctrl> key you can select several individual objects.
Once you have made your selection, then click on 'OK'. The Print dialog box appears. You can determine the layout of the pages to be printed with 'File' 'Printer setup'.