'Extras' 'Accept change'Permalink

Shortcut: <Space>

This command is available in the compare mode.

⮫ “'Project' 'Compare'”

For all units, which are cohering with that one where the cursor currently is placed, and which have the same sort of difference marking, (e.g. subsequent lines), the version of the reference project will be accepted for the actual project (only possible in this direction!). The corresponding units will be shown (with the corresponding coloring) in the left side of the window.

⮫ “Execute comparison”

For accepting changes of particular units please use 'Accept changed item'.

⮫ “'Extras' 'Accept changed item'”

The acceptance of different project parts (differences) or access right properties is only possible from the reference project of the actual project, not vice versa.