'Extras' 'Accept changed item'Permalink

Shortcut: <Ctrl> <Spacebar>

This command is available in the compare mode.

⮫ “'Project' 'Compare'”

Only the single unit (line, network, element) where the cursor is currently placed, will be accepted for the actual version. The corresponding units will be shown (with the corresponding coloring) in the left side of the window.

⮫ “Execute comparison”

If for a POU, which has got marked red-colored in the structure tree because of a change of its content, this change gets accepted, then the POU will be indicated by yellow coloring in the actual project.

POUs which are only available in the current project because of 'Accept changed item', also will be indicated by yellow coloring. POUs which have been removed from the current project because of 'Accept changed item', will be indicated by yellow coloring in the reference project.

⮫ “Execute comparison”

The acceptance of different project parts (differences) or access right properties is only possible from the reference project of the actual project, not vice versa.