Execution of update via memory cardPermalink

Boot project and firmware update

Precondition: Prepared memory card with boot project and firmware.

⮫ “Preparation of memory card”

  1. Switch off the device.

  2. Insert the memory card.

  3. Switch on the device.

    Alternating flashing of the RUN and ERR LEDs indicates that the update process is running.

    At the end of the update process, a reboot is executed and the boot project and system firmware are started to complete the update process.

    If the RUN LED blinks (ERR LED is off), the update was successful and the display shows “done”.

    If the ERR LED blinks (RUN LED is off), the update failed and the display shows “FAIL”.

    The text file “SDCARD.RDY” contains the results of the individual updates. If the update fails, the file contains the reasons for the abort. Based on this information, further steps can be taken to resolve the problem.

  4. Switch off the device.

  5. Remove the memory card.

  6. Switch on the device.

    The system starts with the new boot project and firmware.

Firmware update

Precondition: Prepared memory card with boot project and firmware.

⮫ “Preparation of memory card”

  1. Switch off the device.

  2. Insert the memory card.

  3. Switch on the device.

    Alternating flashing of the RUN and the ERR LED indicates that the update process is running.

    At the end of the update process, a reboot is executed and the system firmware is started for the finishing of the update process.

    If the RUN LED blinks (ERR LED is off), the update was successful and the display shows done.

    If the ERR LED blinks (RUN LED is off), the update failed and the display shows FAIL.

    The text file “SDCARD.RDY” contains the results of the individual updates. If the update fails, the file contains the reasons for the abort. Based on this information, further steps can be taken to resolve the problem.

  4. Switch off the device.

  5. Remove the memory card.

  6. Switch on the device.

    The system starts with the new firmware.