BITADRPermalink

IEC operator: Address function not prescribed by the standard IEC 61131-3.

⮫ “Overview”

BITADR returns the bit offset within the segment in a DWORD. Note that the offset value depends on whether the option byte addressing in the target settings is activated or not.

VAR
 var1 AT %IX2.3:BOOL;
 bitoffset: DWORD;
END_VAR

Example in ST:

‎ bitoffset:=BITADR(var1); (* Result if byte addressing=TRUE: 19, if byte addressing=FALSE: 35 *)‎

NOTICE

NOTICE
NOTICE
NOTICE

NOTICE

NOTICE

After an Online Change there might be changes concerning the data on certain addresses. Please regard this in case of using pointers on addresses.