Command 'Import project to SVN'Permalink

Symbol: _svn_icon_import

Function: This command opens the “Import Project to SVN” dialog for importing a CODESYS project to the SVN repository.

Call: Menu bar: “Project  SVN”.

Requirement

  • You have access to an SVN repository and you know its URL.

  • You have read access to the entire project.

NOTICE

NOTICE
NOTICE
NOTICE

NOTICE

NOTICE

Projects are always saved unencrypted on the server. Therefore, take appropriate security measures (for example, respective access rights to the SVN server) for protecting your projects.

See also

Dialog 'Import Project to SVN'

“URL of SVN repository”

URL of the SVN repository with the new project folder where the files are imported

Example: ‎https://svnserver/repository/trunk/ControlABC.project‎

Hint: When importing libraries, specify the extension ‎.library‎ or ‎_library‎. For projects, specify the extension ‎.project‎ or ‎_project‎. Then the project type is recognized automatically at checkout and the options are set accordingly in the “Checkout” dialog.

_svn_button_three_dots

Opens the “SVN Repository Browser” dialog The previous project structure is displayed and you can edit them here.

“Import message”

Text for use as log message

Example: ‎Control project for customer A‎

“Recent messages”

Opens the “Recent Messages” dialog. There you can reuse the last log messages.

“Generate SVN_VERSION_INFO”

_cds_icon_option_deactivated: The object ‎SVN_VERSION_INFO‎ is not created automatically during the import operation. Therefore, the project does not get any global constants or variables for the project metadata.

“OK”

Creates the current project in the SVN repository and imports the project objects. The local project in Automation Builder is linked to the SVN repository. Overlay icons show this in the object trees.