Overlay IconsPermalink

Every object in CODESYS has a status value in the SVN repository. This status value is displayed in the object tree (in the “POUs”, “Devices”, or “Modules” views) for each object by overlay icons.

Table 937: Overlay icons

_svn_icon_status_added

Object is planned to be added to the SVN repository.

_svn_icon_status_conflicted

Object conflicted

_svn_icon_status_deleted

Object deleted

_svn_icon_status_modified

Object modified

_svn_icon_status_modified_properties

Object with modification in the metadata

_svn_icon_status_modified_binary_only

Object with modifications in the memory format

_svn_icon_status_normal

Object normal

_svn_icon_status_readonly

Object write-protected (read-only)

_svn_icon_status_locked

Object locked

_svn_icon_status_deleted_children

Object with deleted subobjects

_svn_icon_status_ignore_on_commit

Object ignored on commit

_svn_icon_status_external

External object

_svn_icon_status_ignored

Ignored object

_svn_icon_status_unversioned

Unversioned object

_svn_icon_status_modified_children

Object with modified subobjects

_svn_icon_status_transient

The object is not saved in the SVN repository. It will be created again when loaded from SVN.

_svn_icon_status_version_info_not_available

‎SVN_VERSION_INFO‎ temporarily unavailable, for example as with interface libraries

_svn_icon_refresh

The status of the object is not updated.

_svn_icon_status_update_available

The object was modified on the server (Update available).

_svn_icon_lock_steal

The object was locked on the server by another user (or in another working directory).

_svn_icon_status_tree_conflict

Tree conflict by changes to the structure of the project