Tab: EtherCAT Master – Parameters Permalink

The tab contains the master parameters defined in the device description file.

When the “auto-configuration mode” is enabled in the “Master” dialog, the parameters are configured automatically according to the device description file and the network topology. The generic editor should not be used to modify these parameters because invalid settings may result in an invalid configuration.

“Value”

Editable: Changes become effective only when the auto-configuration mode is disabled.

Whether a change becomes effective depends on the respective parameter.