Dialog: Customize: Command Icons Permalink

Function: With this dialog, you define the icons of the menu commands.

Call: “Tools  Customize” command, “Command Icons” tab

Table 719: “Command Icons”

“Assign”

Opens a dialog where you can select the new icon (*.ico)

“Remove”

Removes the custom icon

The default icon is active again.

“Reset”

Resets all command icons to the default settings

“Load”

Loads the settings from a stored file (<file name>.opt.keyb)

“Save”

Saves the current settings to a file (<file name>.opt.keyb)

For more information, see: ⮫ “Customizing Command Icons ”