Command 'Bookmarks'Permalink

Symbol: _cds_icon_view_bookmark

Function: This command opens the “Bookmarks” view.

Call: Menu bar: “View”.

_cds_icon_cmd_previous_bookmark“Previous Bookmark”

Jumps to the bookmark that above the selected bookmark in the table and opens the respective POU in the editor.

_cds_icon_cmd_next_bookmark“Next Bookmark”

Jumps to the bookmark that below the selected bookmark in the table and opens the respective POU in the editor.

_cds_icon_delete_from_llist

Deletes the selected bookmark from the table and in the respective POU.

List of bookmarks in the project with the following information: “Bookmark”, “Object”, and “Position”.

You can edit the bookmark order per drag&drop.

When you double-click a row, CODESYS opens the respective “Object” in the editor and jumps to this bookmark.

“Bookmark”

Name of the bookmark as assigned by CODESYS in ascending numerical order: “Bookmark_0”, “Bookmark_2” etc.

If the bookmark is selected and you click in the field, then it is editable and you can modify the bookmark name.

“Object”

Name and project path of the POU where the bookmark is set

Example: ‎POU_Add [PLC_1: SPS-Logic: Application]‎

“Position”

Position of the bookmark in the POU

Example: ‎Row 3, Column 1 (Impl)‎

‎(Impl)‎: in the implementation part of the POU

‎(Decl)‎: in the declaration part of the POU