The pragma {attribute 'parameterstringof'}
allows that the instance name of the specified parameter is made accessible for
the referenced visualization. An interface variable (STRING
) will contain the instance name of the specified parameter. The interface variable
is visible within the referenced visualization and can for example be used in a text
output.
Syntax:
{attribute 'parameterstringof' := '<variable>'}
Example: declaration of a interface
VAR_INPUT {attribute 'parameterstringof' := 'iftDut_A'} sItfNameDut_A: STRING; END_VAR VAR_IN_OUT iftDut_A : DUT_A; END_VAR