Symbol:
; keyboard shortcut: [Alt]+[F6].
Function: The command opens and closes the “Interface Editor” tab above the visualization editor.
Call: Menu bar: “Visualization Interface Editor” Also by clicking on the small down arrow at the top of the visualization editor
Tab 'Interface Editor'
Symbol: 
The tab contains an editor for the declaration of interface variables. The editor behaves in a similar way to the declaration editor of a function block, however interface variables are not initialized.
Syntax
<scope>
( {attribute '<attribute name>' ( := '<expression>' )? } )?
<identifier> : <data type>;
END_VAR
<scope> : VAR_INPUT | VAR_OUTPUT | VAR_IN_OUT
// (...)? : Optional
Example
Declaration in the interface editor
VAR_INPUT
{attribute 'parameterstringof'}
sIdentifier : STRING; // String for instance name
iCounter : INT;
END_VAR
VAR_IN_OUT
{attribute 'VAR_IN_OUT_AS_POINTER'}
fbController: FB_Controller;
END_VAR
Scopes
Possible scopes for interfaces of visualizations or dialogs
|
|
Note: In the case of dialogs, the data is written back only when the dialog is closed. Hint: We strongly recommend that you use this scope so that the return of values is possible. Moreover, no data needs to be copied. |
|
Pragma |
When transferring a pointer to a data object In contrast to the Note: Use this scope only if the visualization implements a Dialog. |
|
|
When transferring data that will only be read Note:
|
|
Pragma |
When transferring a variable (data type |