You can configure a user input for a visualization that causes a referenced visualization to open as a dialog. For example, a user clicks on a button, whereupon a dialog opens requesting the input of values. A dialog is used to collect user inputs and, if it is modal, it can lead to inputs outside the dialog being blocked.
Only visualizations with the visualization type “Dialog” can be opened as dialog. The visualization type is configured in the dialog “Properties” of a visualization object.
Basic procedure:
Requirement: The project contains a main visualization and a dialog.
-
Configure a user input for the main visualization with the action “OpenDialog” for the dialog.
The opening of the dialog is configured.
-
Configure a user input for an element of the dialog with the action “CloseDialog”.
Hint: in the case of non-modal dialogs you can also configure the user input for closing outside the dialog.
The closing of the dialog is configured.
You can also use dialogs from the library instead of self-made dialogs. For example,
if the library VisuDialogs
is integrated in the project, you can use the dialogs VisuDialogs.Login
or VisuDialogs.FileOpenSave
contained in it.
Configuring a visualization object as a dialog
-
Select the object in the view “Devices”, open the context menu and select the command “Properties”.
-
Select the tab “Visualization”.
-
Activate the option “Dialog” and close the dialog with “OK”.
The visualization has the visualization type “Dialog” and can be called as such.
Configuring a dialog call
When calling a dialog, a user normally clicks on a button, whereupon a dialog opens requesting an input.
In the following example, a dialog representing a calendar enables a date to be entered.
Requirement: The project contains the visualizations visMain
and dlgCalender
.
-
Set the visualization type of
dlgCalender
to Dialog. -
Drag a rectangle into the visualization
visMain
. -
Configure the property “Texts Text” with the text
Due Date: %t[yyyy-MM-dd]
.Configure the property “Text variables Text variable” with
PLC_PRG.dateDue
. -
Drag a button into the visualization.
-
Configure the property “Texts Text” with the text
Open dialog
.Configure the property “Input configuration OnMouseClick” for the action “Open Dialog” with
dlgCalender
.The user input for the opening of the dialog is configured.
-
Double-click on the dialog
dlgCalender
. -
Drag the element “Date picker” into the visualization editor.
-
Configure the property “Texts Text” with
Due Date: %t[yyyy-MM-dd]
.Configure the property “Variable” with
PLC_PRG.dateCalender
.The element is configured.
-
Drag a button into the visualization editor.
-
Configure the property “Texts Text” with
OK
: -
Configure the property “Input configuration OnMouseClick”for the action “Close Dialog ”with
dlgCalender, Result: OK
. -
Configure a further property “Input configuration OnMouseClick” for the action “Execute ST-Code” with
PLC_PRG.dateDue := PLC_PRG.dateCalendar;
.The user input for the closing of the dialog is configured.
-
Drag a further button into the visualization editor.
-
Configure the property “Texts Text” with
Cancel
: -
Configure the property “Input configuration OnMouseClick” for the action “Close Dialog ”with
dlgCalender, Result: Cancel
. -
The user input for the cancellation of the dialog is configured.
-
Compile, load and start the application.
Variable declaration:
PROGRAM PLC_PRG VAR dateDue : DATE := DATE#2000-01-01; dateCalendar : DATE; END_VAR
Opening a dialog globally
Normally a dialog appears only on the display variant on which the user has executed the triggering event.
However, you can configure the opening of the dialog in such a way that the dialog appears simultaneously on all active display variants configured under the visualization manager. This way, for example, an input request can appear simultaneously on all display variants although a user only entered something on the CODESYS TargetVisu.
If a user closes the dialog on a CODESYS TargetVisu display variant, it will be closed on all display variants.
You can open and close a global dialog with the functions OpenDialog3
and CloseDialog2
from the library VisuElems
.
Implementing an application access to a dialog
In the application code you can implement the access to a dialog that is managed in the dialog manager. The dialog manager automatically instances and manages all visualizations of the type “Dialog”. The access takes place via the internal visualization manager.
First of all, implement the access to the dialog manager by calling the GetDialogManager()
method of the internal visualization manager. You can then use the methods of the
dialog manager to program the program sequence of a dialog.
In the following example a button is configured so that it opens the preconfigured
dialog Login
when clicked on. The user can enter a name and a password in the dialog. The dialog
Login
is contained in the library VisuDialogs
. You can also call a self-made dialog in the same way.
Implementing an application access to the dialog Login
from the library VisuDialogs
:
Requirement: The library VisuDialogs
is integrated in the project.
-
Insert a new visualization
visMain
under the application.The visualization editor opens.
-
Drag a button into the visualization editor.
-
Enter in its property “Text”
Login
.The button is labelled.
-
Click on “Configure ”in the property “Input configuration OnMouseDown”.
-
Select the input action “Execute ST-Code” and click on
.
-
Enter the following function call in the ST editor:
OpenLoginDialog(pClientData);
The main visualization contains a button. If a user clicks on the button, the dialog
Login
opens and the functionOpenLoginDialog()
is called. -
Click on “Configure ”in the property “Input configuration OnDialogClosed”.
-
Select the input action “Execute ST-Code” and click on
.
-
Enter the following function call in the ST editor:
OnLoginDialogClosed(pClientData);
If a user closes the dialog, the function
OnLoginDialogClosed()
is called.
Implementation of the function OpenLoginDialog():
FUNCTION OpenLoginDialog : BOOL VAR_INPUT pClientData : POINTER TO VisuStructClientData; END_VAR VAR dialogMan : IDialogManager; loginDialog : IVisualisationDialog; pLoginInfo : POINTER TO Login_VISU_STRUCT; // Login_VISU_STRUCT contains the parameters defined in the interface of visualization "Login". result : Visu_DialogResult; stTitle : STRING := 'Login ...'; stPasswordLabelText: STRING; stUserLabelText: STRING; stUsername: STRING; END_VAR dialogMan := g_VisuManager.GetDialogManager(); // The DialogManager is provided via the implicitly available VisuManager IF dialogMan <> 0 AND pClientData <> 0 THEN loginDialog := dialogMan.GetDialog('VisuDialogs.Login'); // Dialog to be opened is specified IF loginDialog <> 0 THEN pLoginInfo := dialogMan.GetClientInterface(loginDialog, pClientData); IF pLoginInfo <> 0 THEN // In the following the parameters of the login dialog in the Login_VISU_STRUCT will be read pLoginInfo^.stTitle := stTitle; pLoginInfo^.stPasswordLabelTxt := stPasswordLabelText; pLoginInfo^.stUserLabelTxt := stUserLabelText; dialogMan.OpenDialog(loginDialog, pClientData, TRUE, 0); END_IF END_IF END_IF
OnLoginDialogClosed()
defines the reaction to the closing of a dialog.
Implementation of the function OnLoginDialogClosed()
:
FUNCTION OnLoginDialogClosed : BOOL VAR_INPUT pClientData : POINTER TO VisuStructClientData; END_VAR VAR dialogMan : IDialogManager; loginDialog : IVisualisationDialog; pLoginInfo : POINTER TO Login_VISU_STRUCT; result : Visu_DialogResult; stPassword: STRING; stUsername: STRING; END_VAR dialogMan := g_VisuManager.GetDialogManager(); // The DialogManager is provided via the implicitly available VisuManager IF dialogMan <> 0 AND pVisuClient <> 0 THEN loginDialog := dialogMan.GetDialog('VisuDialogs.Login'); // Gets the login dialog IF loginDialog <> 0 THEN result := loginDialog.GetResult(); // Gets the result (OK, Cancel) of the dialog IF result = Visu_DialogResult.OK THEN loginDialog.SetResult(Visu_DialogResult.None); // Reset to default (none) pLoginInfo := dialogMan.GetClientInterface(loginDialog, pVisuClient); // Structure Login_VISU_STRUCT gets read; // In the following the structure parameters can be set IF pLoginInfo <> 0 THEN stPassword := pLoginInfo^.stPasswordpLoginInfo^.stPassword := ''; // Reset the passwword stUsername := pLoginInfo^.stUsername; END_IF ELSIF result = Visu_DialogResult.Cancel THEN loginDialog.SetResult(Visu_DialogResult.None); // React on 'Cancel' ELSE // nothing to do END_IF END_IF END_IF
See also