Constant variables are declared in global variable lists or in the declaration part of programming objects. In implementations, constant variables can be accessed as read-only via the instance path.
Syntax
<scope> CONSTANT <identifier> : <data type> := <initial value> ; END_VAR <scope> : VAR | VAR_INPUT | VAR_STAT | VAR_GLOBAL <data type>: <elementary data type> | <user defined data type> | <function block> <initial value> : <literal value> | <identifier> | <expression>
Always assign an initialization value when declaring a constant variable. Then the constant cannot be written any more.
Example
Declaration
VAR CONSTANT c_rTAXFACTOR : REAL := 1.19; END_VAR
Call
rPrice := rValue * c_rTAXFACTOR;
You have read-only access to constant variables in an implementation. Constant variables are located to the right of the assignment operator.