The IEC operator is used for converting the REAL
data type into the DINT
data type. CODESYS takes only the integer part of the number.
In CoDeSys V2.3, the TRUNC
operator converts REAL
into INT
. If you import a V2.3 project, then CODESYS automatically replaces TRUNC
with TRUNC_INT
.
If CODESYS cannot represent the input value by a DINT
or INT
, then the result of this function is undefined. The behavior of such input values
is platform-dependent.




NOTICE

If the operand value for a type conversion operator is outside of the value range
of the target data type, then the result output depends on the processor type and
is therefore undefined. This is the case, for example, when a negative operand value
is converted from LREAL
to the target data type UINT
.
Information can be lost when converting from larger data types to smaller data types.
Examples
Result in diVar
: 1
ST
diVar := TRUNC(1.9); (* Result: 1 *) diVar := TRUNC(-1.4); (* Result: -1 *)
See also