NOTICE

If the operand value for a type conversion operator is outside of the value range
of the target data type, then the result output depends on the processor type and
is therefore undefined. This is the case, for example, when a negative operand value
is converted from LREAL to the target data type UINT.
Information can be lost when converting from larger data types to smaller data types.
The operators convert time values (TIME or LIME) into the specified data types and return this type-converted value.
Call syntax
<variable name> := <time conversion operator> ( <operand> ); <operand> = <variable name> | <literal>
Operators
TIME_TO___UXINT TIME_TO___XINT TIME_TO___XWORD TIME_TO_BIT TIME_TO_BOOL TIME_TO_BYTE TIME_TO_DATE TIME_TO_DINT TIME_TO_DT TIME_TO_DWORD TIME_TO_INT TIME_TO_LDATE TIME_TO_LDINT TIME_TO_LINT TIME_TO_LREAL TIME_TO_LTIME TIME_TO_LTOD TIME_TO_LWORD TIME_TO_REAL TIME_TO_SINT TIME_TO_STRING TIME_TO_TOD TIME_TO_UDINT TIME_TO_UINT TIME_TO_ULINT TIME_TO_USINT TIME_TO_WORD TIME_TO_WSTRING LTIME_TO___UXINT LTIME_TO___XINT LTIME_TO___XWORD LTIME_TO_BIT LTIME_TO_BOOL LTIME_TO_BYTE LTIME_TO_DATE LTIME_TO_DINT LTIME_TO_DT LTIME_TO_DWORD LTIME_TO_INT LTIME_TO_LDATE LTIME_TO_LDINT LTIME_TO_LINT LTIME_TO_LREAL LTIME_TO_LTOD LTIME_TO_LWORD LTIME_TO_REAL LTIME_TO_SINT LTIME_TO_STRING LTIME_TO_TIME LTIME_TO_TOD LTIME_TO_UDINT LTIME_TO_UINT LTIME_TO_ULINT LTIME_TO_USINT LTIME_TO_WORD LTIME_TO_WSTRING
Converting to Boolean values
The operator returns FALSE if and only if the operand value can be interpreted as "0".
|
|
|
|
|
|
|
|
|
|
|
|
Converting to a string




NOTICE

String manipulation when converting to STRING or WSTRING
When converting the type to STRING or WSTRING, the typed value is left-aligned as a character string and truncated if it is too
long. Therefore, declare the return variable for the type conversion operators <>_TO_STRING and <>_TO_WSTRING long enough that the character string has enough space without any manipulation.
|
|
|
|
|
|
Examples
ST implementation language
FUNCTION_BLOCK FB_ConvertTimeAndDate VAR_INPUT END_VAR VAR_OUTPUT END_VAR VAR ltReturn_1: LTIME; lwReturn_2: LWORD; rReturn_3: REAL; strReturn_4: STRING; timReturn_5: TIME; todReturn_6: TIME_OF_DAY; uliReurn_7: ULINT; wstrReturn_8: WSTRING; wstrReturn_80: WSTRING; uliReurn_70: ULINT; todReturn_60: TIME_OF_DAY; timReturn_50: TIME; strReturn_40: STRING; rReturn_30: REAL; lwReturn_20: LWORD; ltReturn_10: LTIME; ltReturn_11: LTIME; lwReturn_21: LWORD; rReturn_31: REAL; strReturn_41: STRING; timReturn_51: TIME; todRedurn_61: TIME_OF_DAY; uliReurn_71: ULINT; wstrReturn_81: WSTRING; ltReturn_12: LTIME; xReturn_9: BOOL; xReturn_90: BOOL; xReturn_91: BOOL; xReturn_92: BOOL; dateReturn_6: DATE; timReturn_60: TIME; wReturn_61: WORD; todReturn_61: TIME_OF_DAY; END_VAR ltReturn_1 := DT_TO_LTIME(DT#2019-9-9-23:59:59); ltReturn_10 := DT_TO_LTIME(DT#1970-1-1-0:0:0); ltReturn_11 := DT_TO_LTIME(DT#1970-1-2-0:0:1); ltReturn_12 := DT_TO_LTIME(DT#1970-1-3-12:30:30); lwReturn_2 := TIME_TO_LWORD(T#5D4H2M3S2MS); lwReturn_20 := TIME_TO_LWORD(T#0D0H0M0S0MS); rReturn_3 := TIME_TO_REAL(T#5D4H2M3S2MS); rReturn_30 := TIME_TO_REAL(T#0D0H0M0S0MS); strREturn_4 := TIME_TO_STRING(T#5D4H2M3S2MS); strREturn_40 := TIME_TO_STRING(T#0D0H0M0S0MS); timReturn_5 := TOD_TO_TIME(TOD#23:59:59.999); timReturn_50 := TOD_TO_TIME(TOD#0:0:0.000); timReturn_51 := TOD_TO_TIME(TOD#0:0:0.001); dateReturn_6 := TOD_TO_DATE(TOD#23:59:59.999); timReturn_60 := TOD_TO_TIME(TOD#0:0:0.000); wReturn_61 := TOD_TO_WORD(TOD#0:0:0.001); uliReurn_7 := DATE_TO_ULINT(D#2019-9-9); uliReurn_70 := DATE_TO_ULINT(D#1970-1-1); uliReurn_71 := DATE_TO_ULINT(D#1970-1-2); wstrReturn_8 := DATE_TO_WSTRING(D#2019-9-9); wstrReturn_80 := DATE_TO_WSTRING(D#1970-1-1); wstrReturn_81 := DATE_TO_WSTRING(D#1970-1-2); xReturn_9 := DATE_TO_BOOL(D#2019-9-9); xReturn_90 := DATE_TO_BOOL(D#1970-1-1); xReturn_91 := DATE_TO_BOOL(D#1970-1-2); xReturn_92 := DATE_TO_BOOL(D#1970-1-3);


FBD implementation language