This operator is an extension of the IEC 61131-3 standard.
The operator is used for checking whether a reference refers to a valid value. For
a description of use and an example, refer to the description for the REFERENCE data type.
See also