NOTICE

Implement concurrent bit access by two tasks only if the processor can execute bit access directly on the memory. All x86 and x64 systems have commands for bit access in memory. Systems such as ARM and PPC cannot access bits directly in the memory.
If two tasks execute bit access simultaneously, even though the processor cannot perform
bit access directly in the memory, then proceed as follows. Use a semaphore (SysSemEnter) or a similar technique to prevent competing bit access. However, it is best to execute
the bit access within a task.
With index access, individual bits can be addressed in integer variables. Using a structure variable or a function block instance, individual bits can be addressed symbolically.
Index access to bits integer variables
You can address individual bits in integer variables. To do this, append the variable with a dot and the index of the addressed bit. The bit-index can be given by any constant. Indexing is 0-based.
Syntax
<integer variable name> . <index> <integer data type> = BYTE | WORD | DWORD | LWORD | SINT | USINT | INT | UINT | DINT | UDINT | LINT | ULINT
Example
In the program, the third bit of the variable wA is set to the value of variable xB. The constant c_usiENABLE acts as an index to access the third bit of the variable iX.
Index access
PROGRAM PLC_PRG VAR wA : WORD := 16#FFFF; xB : BOOL := 0; END_VAR // Index access in an integer variable wA.2 := xB;
Result: wA = 2#1111_1111_1111_1011 = 16#FFFB
Constant as index
// GVL declaration VAR_GLOBAL CONSTANT gc_usiENABLE : USINT := 2; END_VAR PROGRAM PLC_PRG VAR iX : INT := 0; END_VAR // Constant as index iX.gc_usiENABLE := TRUE; // Third bit in iX is set TRUE
Result: iX = 4
Symbolic bit access in structure variables
With the BIT data type, you can combine individual bits into a structure and then access them
individually. Then the bit is addressed with the component name.
Example
Type declaration of the structure:
TYPE S_CONTROLLER : STRUCT bitOperationEnabled : BIT; bitSwitchOnActive : BIT; bitEnableOperation : BIT; bitError : BIT; bitVoltageEnabled : BIT; bitQuickStop : BIT; bitSwitchOnLocked : BIT; bitWarning : BIT; END_STRUCT END_TYPE
Declaration and write access to a bit:
PROGRAM PLC_PRG VAR ControlDriveA : S_CONTROLLER; END_VAR // Symbolic bit access to bitEnableOperation ControlDriveA.bitEnableOperation := TRUE;
Symbolic bit access in function block instances
In function blocks, you can declare variables for individual bits.
Example
FUNCTION_BLOCK FB_Controller VAR_INPUT bitSwitchOnActive : BIT; bitEnableOperation : BIT; bitVoltageEnabled : BIT; bitQuickStop : BIT; bitSwitchOnLocked : BIT; END_VAR VAR_OUTPUT bitOperationEnabled : BIT; bitError : BIT; bitWarning : BIT; END_VAR VAR END_VAR ; PROGRAM PLC_PRG VAR fbController : FB_Controller; END_VAR // Symbolic bit access to bitSwitchOnActive fbController(bitSwitchOnActive := TRUE);