CODESYS provides the following integer data types.
|
Data Type |
Lower Limit |
Upper Limit |
Memory |
|---|---|---|---|
|
BYTE |
0 |
255 |
8 bit |
|
WORD |
0 |
65535 |
16 bit |
|
DWORD |
0 |
4294967295 |
32 bit |
|
LWORD |
0 |
264-1 |
64 bit |
|
SINT |
-128 |
127 |
8 bit |
|
USINT |
0 |
255 |
8 bit |
|
INT |
-32768 |
32767 |
16 bit |
|
UINT |
0 |
65535 |
16 bit |
|
DINT |
-2147483648 |
2147483647 |
32 bit |
|
UDINT |
0 |
4294967295 |
32 bit |
|
LINT |
-263 |
263-1 |
64 bit |
|
ULINT |
0 |
264-1 |
64 bit |




NOTICE

Information can be lost when converting from larger to smaller types.
See also