If the device supports the network functionality, then the current network settings for a GNVL (global network variable list) can be displayed and changed in the “Properties” dialog of the object. These are the settings that were used when adding the GNVL in the “Add Network Variable List (Receiver)” dialog.
See also