Symbol: 
The object is used for listing the received network variables and displaying the information: network and transmit information and sender.
You add the object to an application by clicking “Add Object Network Variable List (Receiver)”.
The network variable list (receiver) shows the received network variables, which were declared in network variable list (sender) of another device or project. You cannot change the network variables in the object editor.
The object editor consists of two parts:
-
Information about the sender and transfer log of the list
-
List of declarations of network variables
Dialog Box 'Add Network Variable List (Receiver)'
Function: This dialog box defines the receiver NVL to a sender NVL and adds the receiver NVL to the application object in the device tree.
Call: Main menu “Project Add Object Network Variable List (Receiver)” (when the application object is selected).
|
“Task” |
Task of the current application that controls the variables to be received. |
|
“Sender” |
Drop-down list
|
|
“Import from file” |
File name in “GVL export file *.gvl” format if you have selected “Import from file” for “Sender ”. |