Function: The dialog allows for setting the basic properties of the selected image pool.
Call: “View Properties” of an “Image Pool” object type; context menu of an “Image Pool” object type.
“Download only used images” |
|
“Download by visualization” |
|
“Internal” |
|
“Mark library as symbol library” |
Marks the image pool as a symbol library for use in a visualization. The symbol library
receives the key Requirement: A library project is open. CODESYS displays symbol libraries that are installed in the repository in the “Project Settings” (“Visualization” category, “Symbol Libraries” tab). |
“Textlist for symbol translation” |
Select the text list from the drop-down list that contains the translated texts for the image pool. |