Function: This dialog restricts the range of array elements whose values are displayed during monitoring.
Call: Click in the column field “Data Type” that belongs to the array variable.
Requirement: A POU is in online mode and is being monitored. In addition, a variable of the POU has the data type “ARRAY”.
| “Valid range” | The validity range of the array elements that are monitored. Example of a three-dimensional array:  | 
| “Maximum number of array elements” | Number of elements of the array variables Example:  | 
| When you edit one of the settings “Start”, “End”, or “Scroll range of 1000 elements”, both of the other settings are adapted automatically. | |
| “Start” | Index of the first array element whose value is displayed. | 
| “End” | Index of the last array element whose value is displayed. | 
| “Scroll range of 1000 elements” | Scrollbar for selecting a range from the set of array elements. |