Function: This command halts the application where the error is located despite a programmed exception handling.
Call: This command is not available by default, but it can be configured from the “Tools Customize”, “Add Command” dialog box (“Online” category).
Requirement: The application is in online mode and contains a programmed exception handling with
the __TRY and __CATCH operators.
If you have configured this command from the “Online” menu and you call it from there, then the currently active application is affected. Furthermore, this command can help you to detect errors.