Symbol: 
Function: This command switches between the currently set project localization and the <original version>.
Call: Menu bar: “Project Project Localization”; button in the “Manage Localizations” dialog;
button on the toolbar.
Requirement: A project is open. A default localization for the project is defined in the “Manage Localizations” dialog.
See also
-
Help about CODESYS Visualization: Multi-language capability