Function: This command opens the “Manage localizations” dialog. Select the desired localization language in the dialog or the original version
of the project. You can still accept the localization files *.<language>.po into the project or remove them.
Call: Menu bar: “Project Project localization”.
Requirement: A project is open.
Dialog 'Manage localizations'
|
“Available Localizations” |
List of the localization files available in the project. Example:
The original version is always available. The project can be edited only in the original version. |
|
“Add” |
This button opens the dialog for selecting an additional |
|
“Remove” |
This button removes the |
|
“Default localization” |
|
|
“Switch Localization” |
Use this button to switch to the selected localization. |
|
“OK” |
The project is displayed in the language that is provided by the file selected below the files. If you select “<original version>”, then the project appears in the editable non-localized version. |
See also
: The selected localization is for the default localization. The entry is display
in bold.