Function: The command opens the default dialog for saving a file to the local file system.
The filter is set to file format CSV
. After specifying a name and a location, CODESYS stores the I/O mapping configuration in a CSV
file with the semicolon separator.
Call: Context menu of a device object in the “Devices” view.
Requirement: A device object with an I/O mapping configuration is selected in the device tree.
Parameter names that are not unique are numbered sequentially in this file (@<n>
).