Symbol:
; keyboard shortcut : [Ctrl]+[M] (to toggle between “S”, “R”, “REF”, and None)
Function: The command assigns a reference to an “Output” element.
Call: Menu bar: “CFC Set/Reset”; context menu: “Set/Reset”
Requirements: A CFC editor is active. The input of an “Output” element is selected.
Example:
Declaration:
ref_int : REFERENCE TO INT; a : INT;
CFC:

This corresponds to the ST code: ref_int REF= a;
For more information, see the description for the data type REFERENCE TO.