The Tab “Task Deployment” of the device editor indicates in an overview the tasks that process the individual inputs and outputs of the I/O mapping of your application and the priority with which they do so. You can check here whether an unintentional overwriting of values is caused, which can lead to undefined values.
-
Generate code for the application: to do this select, for example, the command “Build Generate Code”.
-
Open the device editor by double-clicking on the device object in the device tree. Select the “Task Deployment” tab.
You obtain a display of the inputs and outputs of your application and the assignment of the tasks and their priorities. See the description of the “Task Deployment” tab for details.